This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5510: SLAA514 : size of output file

Part Number: MSP430F5510

Tool/software: Code Composer Studio

In SLAA514, chapter 5.2 report the memory footprint of USB keyboard, that is

Code : 7626 bytes

Constants 1096 bytes

Data 679 bytes

Building the project with CCSv7 I have an output file USB_kbd.out of 182 kB, with the following level of optimisation

4 -Whole programs optimization

1 - speed vs size trade off

Does USB_kbd.out (182kB) fit in the internal memory of MSP430F5510 ?

What kind of output format I should select for this purpose to have the memory footprint above ?

Adamo