This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
With CCSv4.1, in C/C++ Project window, under the project name, there is a branch called "Includes", in it, there is one folder (bios_5_30\packages) that is inherited from the migration process, and also an empty folder, is it possible to remove them ? or I have to edit .cdtbuild manually ?
Thanks,
Yuhua
Yuhua,
The directories listed there are defined by the compiler include directories, therefore you can remove unused directories from there simply by right-clicking on the project --> select Build Properties --> Under Compiler you select Include Options.
Hope this helps,
Rafael
Thanks, Rafael,
I understand that C/C++ Projects --> "project name" --> Includes reflect the settings on "project name" -->Build Properities --> C/C++ Build --> Compiler --> Include Options, however, there is no bios_5_30\packages in "Include Options", to remove it, I simply edit file .cdtbuild and delete the following line:
<listOptionValue builtIn="false" value=""${CCSv3_INSTALL_ROOT}/bios_5_30/packages""/>
Somehow this line was set during the "Import Legacy Project" -- I guess small tweak is needed in migration.
I also find out that the empty folder in "Includes" branch is "${COMMON_ROOT}", which is okay.
Yuhua