Step from previous line to the current line and the disassembler window displays all 'BRA @PC' instructions which is incorrect. See 1st screen capture.
The workaround.... scroll the disassembler window up and down or flip to another application and come back. The disassembler window contents is as expected. See second screen capture.
Using code composer version 4.2.0 on Windows XP. Target is MSP430F5438. If relevant it's a large application - see PC is at 0x31520
If firefox, I use right click 'view image' to see the screen captures below clearly.
PS. TI, like the addition of the Problems tab in version 4. Good idea.