Part Number: AM5746
Tool/software: Code Composer Studio
Hi TI Experts.
As I reported to it on other thread, not work the Cross-Trigger in case of using the AM574x IDK.
When set the sync group, CCS showed the error as below. Would you please teach us the reason why this problem happen?
************
CortexA15_0: Trouble configuring cross triggering: Error enabling this function: There is no AET resource to support this job.
CortexA15_1: Trouble configuring cross triggering: Error enabling this function: There is no AET resource to support this job.
************
Here is the reproduced way.
1. Sync Group the Target the A15_0 and A15_1
2. Connect the target
3. Load the program(POSIX-SMP) for each core.
4. Run the program.
Note: When I used the AM572xIDK, it was worked well.
CCS: 8.1.0.00011
If you have any questions, please let me know.
Best regards.
Kaka