Tool/software: Code Composer Studio
I was install CCSv8 to my PC.
but CCSv8 not work.
run CCSv8 show just minute and disappear program.
v8,v7 all version same.
my PC : Windows10 pro, 64bit, i7 processor, 16GB ram, use SSD
have solution?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I was install CCSv8 to my PC.
but CCSv8 not work.
run CCSv8 show just minute and disappear program.
v8,v7 all version same.
my PC : Windows10 pro, 64bit, i7 processor, 16GB ram, use SSD
have solution?
Hyun nam Kim said:run CCSv8 show just minute and disappear program.
Does it get to the point where it asks you to select a workspace? If so, could you attach the .log file from the <workspace>/.metadata directory?
Is there any error message generated or does it just simply close without error?
If you are running an anti-virus software, try temporarily disabling it to see if that helps.
It is possible that the installation is corrupt or incomplete. Please check this related post and try reinstalling to a clean empty directory. If the issue still persists, please zip up the /ccsv8/install_logs folder and attach it here. We can look at that to check if the installation went ok.