This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Trouble Installing CCS Version 8.2.0.00007 Under Windows 10

Tool/software: Code Composer Studio

I have downloaded the latest Windows Offline Installer for CCS8.2.0.00007, and the install keeps getting stuck early in the process due to the following error:

An error occured : error deleting "C:/Users/James Baughman/AppData/Local/Temp/ccs_7eaa0cfa-13ba-4a42-63d4-9b350994655d/ccs_error_codes.csv": permission denied

Note that I have disabled Windows Defender anti-virus and Windows Firewall, and unzipped the install folders before starting the install.

I would appreciate any help you can provide, thanks!

  • Hello James,

    first of all, if possible, change your user name to eliminate spaces, white and special characters.
    Eclipse comes from old UNIX/Linux and some of its utilities do not like spaces, etc. within path names.

    If you cannot change your login name:
    1. download offline installer
    2. turn off anti-virus, disconnect network interfaces like LAN, WLAN, tethering via USB, etc.
    3. run offline installer with admin privileges
    4. select c:\ti\ccs820 or like this as an installation folder
    5. always create separate workspaces for different CCS versions.
  • James,

    One additional detail: can you try to open a prompt and invoke the installer with the option --temp C:\temp (or something without spaces on the pathname?)

    C:\Users\user\Downloads\CCS8.2.0.00007_win32>ccs_setup_8.2.0.00007.exe --temp C:\temp

    That should help overcome this issue.

    Hope this helps,
    Rafael