Other Parts Discussed in Thread: BOOSTXL-K350QVG-S1
Tool/software: Code Composer Studio
I am currently working in Code Composer 8.2.0, and I am working on a projecting involving the use of the BOOSTXL-K350QVG-S1 in conjunction with the MSP432P401R Launchpad kit. After searching for countless hours, the only example of source code I could find involving the use of these devices in CCS was the BOOSTXL-K350QVG-S1_GrlibExample_MSP432P401R from the MSP-EXP432P401R_Software_Examples_widows files. However, when I try to import this into my CCS workspace, I get the error message:
"Import failed for project 'BOOSTXL-K350QVG-S1_GrlibExample_MSP432P401R' because its meta-data cannot be interpreted. Please contact support."
I do not have any idea how to fix this. I tried to import this into a version of CCS 6.2.0, but the same error occurs. How can I resolve this issue so I can use this example code with the BOOSTXL device?
If there is no way to fix this particular issue, what I really need is just some information on what needs to be included and how in a CCS project in order to use basic functions from the graphics library used to write to the BOOSTXL screen from the MSP.
I am attaching a zipped version of the project to this post. Thank you for any and all help.