Tool/software: TI C/C++ Compiler
Hi!
I have the following problem:
After 2 years, the battery of my ASUS G53SV given up the ghost and I've bought a new (not a replica but the original model purchased from www.topakku.com/asus-g53sv.html ).
The battery can be used easily and is also recognized by the system.
Only problem: He can not be charged.
When you first insert the battery was at 33%. In network mode, it remains at 33%. However, it is shown: left 33% (network operation is not recharged).
Have already taken out the battery again and blown onto the contacts and everything wiped cloth with NEM (thought it might be a bit dusty). But nothing helps.
Can someone help me? Were so thankful for every tip.