Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Team,
my customer had an automatic update related to EMU_TI 8.0.803.0
getstate - EMU_TI compareversion: 8.0.27.9 8.0.803.0
getstate - New state: feature registered
writeDebugFile - Install Information:
- writeDebugFile - Install Version: 6.1.2.00015
- Install Source : C:/ti/ccsv6/eclipse/downloads
- Install Temp : C:/Users/xxxxxxx/AppData/Local/Temp/ccs_08f434f7-30aa-4107-51fd-49955cfd1e5d
- Install Type : Web
- writeDebugFile - OS : Windows NT
- writeDebugFile - OS Version : 6.2
- writeDebugFile - OS Platform : windows
- writeDebugFile - : 64-bit
ProgressPane::Run - RunInstall C:/ti/ccsv6/eclipse/ccs_config.xml 1 0 0 0 c:/ti/ccsv6/install_logs/ccs_setup_6.1.2.00015_install.log ::progressPane0 -1
Installed is only support for C2000 and TMS470.
Installation done without errors
Now the customer has following error: Launching Debug Session
can not read system setup data file from XML File
C:\\users\users\xxxx\workspace\projectxy.CCX
could not open file
c"\ti\ccs6\ccs_base\common\targetdb\drivers\TI_reg_ids\TMS470R53X_RegIDs.xml
!cleaning or running the project from another path didn't help!
the question here is why EMU_TI should change the configuration of a C2000 project to TMS470??? and how to solve this issue?
Thank you in advance
best regards
karim