Part Number: TMDSLCDK6748
Other Parts Discussed in Thread: TMDSEMU110-U, OMAPL138
Tool/software: Code Composer Studio
Hello,
I am a bigenner and i am using TMDSLCDK6748 platform.
I am trying to create a project with ccs8 and afterthat implement them in the platform. However i have a problem to connect the ccs to the platform, knowing that i am using the J3 (UART2) connection.
My Question is: Can i use the J3 connection to connect the ccs to the platform, and create projects, build them and implement them directly through the USB cable?
Thanks