This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6727: problem with tconf

Part Number: TMS320C6727

Tool/software: Code Composer Studio

CCS Version: 8.1.0.00011

Java 8.191

Bios 5.42.1.09

compiler 7.4.23

I am part of a group where at least 4 others can build from the same project files without problems. I am setting up a new windows 10 computer and can't seem to get past the error during a build shown below. At least one other person in the group recently updated to the same new computer as I have and did not see this problem.

Building file: "C:/CCSws/PHX_GIT/Firmware/Phoenix/Code/DSP/SHARED/5600P1.TCF"

Invoking: TConf

"C:/ti/bios_5_42_01_09/xdctools/tconf" -b -Dconfig.importPath="C:/ti/bios_5_42_01_09/packages;" "C:/CCSws/PHX_GIT/Firmware/Phoenix/Code/DSP/SHARED/5600P1.TCF" "../5600P1.TCF"

subdir_rules.mk:12: recipe for target 'build-1941894959-inproc' failed

C:\ti\bios_5_42_01_09\xdctools\C:/ti/bios_5_42_01_09/xdctools/tconf: can't create session manager: create of JVM failed

gmake[2]: *** [build-1941894959-inproc] Error 1

subdir_rules.mk:9: recipe for target 'build-1941894959' failed

gmake[1]: *** [build-1941894959] Error 2

gmake[1]: Target 'main-build' not remade because of errors.

makefile:266: recipe for target 'all' failed

gmake: *** [all] Error 2

**** Build Finished ****