Part Number: LAUNCHXL-CC2650
Tool/software: Code Composer Studio
Greetings,
I am starting into a ble project, attempting to run your demo.
I have a 2650 launchpad kit and xds110 cable (probably two years old, I admit). I built the ble_sdk_2_2_2_25/simple_peripheral_lp demo, both stack and app. Then I tell CCS to flash the board, but get a red fast flashing led and the error messages below. Tried board reset and usb unplug with no change in results.
Thanks for your help!
-belvin
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Warning: A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect to the debug target. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 8.0.27.9)
IcePick_C: Warning: A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect to the debug target. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 8.0.27.9)
IcePick_C: Warning: The firmware update completed successfully. (Emulation package 8.0.27.9)
Cortex_M3_0: Warning: The firmware update completed successfully. (Emulation package 8.0.27.9)
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.0.27.9)
CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.0.27.9)
CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.0.27.9)
CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.0.27.9)