Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH, CC3220SF
Tool/software: Code Composer Studio
I am not able to connect to a CC3220SF-LAUNCHXL via Code Composer Studio Version: 8.2.0.00007 when I set the SOP config to 001. I am able to connect and program the flash via Uniflash when I set the SOP config to 010.
Here's how I'm testing:
I created a brand new CC3220SF.ccxml file with XDS110 USB debug probe as the debug type and target set to CC3220SF_SWD. When I tested the connection, I am getting this error:
The value is '-615' (0xfffffd99).
The title is 'SC_ERR_SWD_PROTOCOL'.
Can somebody please provide additional troubleshooting steps?
Thanks,
Manish
---------------------
Complete Log:
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\mtalreja\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'May 30 2018'.
The library build time was '23:03:35'.
The library package version is '8.0.27.9'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-615' (0xfffffd99).
The title is 'SC_ERR_SWD_PROTOCOL'.
The explanation is:
The target failed to see a correctly formatted SWD header. The
connection to the target may be unreliable. Try lowering the
TCLK setting before trying again.
[End: Texas Instruments XDS110 USB Debug Probe_0]