Other Parts Discussed in Thread: MOTORWARE, CODECOMPOSER
Tool/software: Code Composer Studio
Please take the following under serious advisement to fix Code Composer so it is more compatible with backing up and project versioning with Git:
1. I suggest creating a folder in C:\ti for your custom projects code based on your preference. Lets say MyName for this discussion
2. Create a Code Composer Workspace folder in that MyName folder to work in
3. Also create folders "C:ti\MyName\inc" and "C:\ti\MyName\src". Custom C files go into the src folder and h files in the inc folder.
4. Your modified User.h from Motorware can go into "C:\ti\MyName\inc" so you can keep the motorware one as original and not use it. Then you have the option of using user.h in your real project(s) later and keeping it under version control without trying to put Motorware or C2000 code into Git. For the TI source code not included in Git, all you have to do is keep a pristine copy of the install files for the version your code will work with. Any modifications to it should not be counted on.
5. You can then have C:\ti\MyName under git version control without adding all the Motorware source files
6. For builds to work, you need to right click each lab project and find the Include Options (like under C2000 Compiler) and select it. Then add C:\ti\MyName\inc to the top of the list so it loads your user.h instead of motorware's when compiling a lab.
7. Note that modifications to Lab C code wont be saved in the Git repository but you should make any serious changes in a C file in C:\ti\MyName\src
PROBLEM that needs fixing in CodeComposer: The Include Options is stored in the wrong place for the labs so it wont be backed up by Git. If I restore the MyName directory on another computer that I have installed CodeComposer on, the C:\ti\MyName\inc is missing from the project properties and have to be re-added. Obviously this setting was not saved in the c:\ti\MyName\Workspace8 like it should have been. This is strange because if you create a new project from scratch, that is exactly where the new project ends up.
Note that it makes no sense to have your workspace under your My Documents folder if you want to share your Workspace with other login accounts.