Part Number: TIDM-BIDIR-400-12
Other Parts Discussed in Thread: TMDSCNCD28035ISO, TMDSCNCD28035
Tool/software: Code Composer Studio
Hello.
I'm trying to make prototype hardware of TIDM-BIDIR-400-12.
I bought TMDSCNCD28035ISO control card from Digikey.
After I attached the card to the PCB board, in ccs, showed an error message.
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 6.0.407.3)
I finally realized that in the original design, they used TMDSCNCD28035, not TMDSCNCD28035ISO.
But, I want to use the board I bought, so I tried to connect the USB to the TMDSCNCD28035ISO directly.
Then ccs showed this message.
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the debug probe connection
may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board).
If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.407.3)
I have a question. those TMDSCNCD28035 and TMDSCNCD28035ISO have same pin feature?
if it is right, could I use TMDSCNCD28035ISO for that original PCB?
I'm not sure I can use or not. and I wonder to know if I attach TMDSCNCD28035, is it work well.
Thanks