This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/BEAGLEBOARD-X15: PRU compiler v2.3.1 shows a "legacy C6000" option in CCS 8.2

Part Number: BEAGLEBOARD-X15
Other Parts Discussed in Thread: AM5728

Tool/software: TI C/C++ Compiler

When setting up an AM5728 PRU project in CCS 8.2.0.00007 using PRU compiler v2.3.1 noticed that in the Miscellaneous options there is a "C6000 legacy mode for performance degradations (-legacy)" option shown:

Not sure if this is a cut-and-paste error in the option description, or that an option for the C6000 compiler is being incorrectly shown for the PRU compiler.