Part Number: TMS320F28022
Tool/software: Code Composer Studio
Win7 SP1 (32bit). CCS 6.1.3. F28022.
Hi CCSrs:
Is there a log file that details what CCS is doing when I change into debug? If so, where is it (are they)?
I have begun to suspect an issue related to erasing the target FLASH, loading the FLASH, and loading the RAM.
Normally, when I click the little spider, a series of windows pops up mentioning stuff about "loading program", "erasing FLASH sector A, B, C..." then "Loading an address range" etc.
The info goes by pretty fast, and I would like to verify these steps in detail.
Any help is appreciated,
Thanks, Mark.