Part Number: AM3359
Tool/software: Code Composer Studio
Hello,
Newbie here, I tried to replicate a bare metal project on beaglebone from this source,
My setup has:
1. Beaglebone with JTAG header soldered
2. XDS100v2 debugger
3. CCS v8
Steps:
1. Create new CCS project, select AM3559 and XDS100v2
2. Compile OK, bbb-test.out file is generated. The program is just a simple while loop counter.
3. Debug configuration, select DebugProbe/CortexA8 , program path: bbb-test.out
Everything else default.
Console error message:
CortxA8: Trouble Writing Memory Block at 0x80000000 on Page 0 of Length 0x900: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9) CortxA8: File Loader: Verification failed: Target failed to write 0x80000000 CortxA8: GEL: File: C:\workspace_v8\test-bbb-jtag\Debug\test-bbb-jtag.out: Load failed.
How do I resolve this error ? I had erased EMMC and got no SD card plugged in. JTAG "test connection" reported no error.
I heard that I need GEL file, is that still needed for CCS v8, if yes where do I get one and why it is not supplied by CCS by default ?
Regards,
AX