Part Number: MSP430FR5994
Tool/software: Code Composer Studio
I´m currently having problems compiling my CCS project.
A few days ago I tried upgrading to CCS version 8.2.0.00007 but it was impossible for me to program with that known C++ indexing bug, so I downgraded to version 8.1.0.00011 again.
Since then I can´t compile my project, following error message appears:
INTERNAL ERROR: C:\ti\ccsv8\tools\compiler\ti-cgt-msp430_18.9.0.STS\bin\acpia430.exe experienced a segmentation fault
while processing function (unknown or file scope) file ../CLoraModule.cpp line 1249
This is caused by a defect in the TI EABI C/C++ Parser.
TI Customer Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Of course I already upgraded the compiler to the newest version, as well as any other software modules except Code Composer itself.
I also tried creating a new project and importing all .cpp and .h files, re-installing CCS and restarting my PC.
The full error message is added here:
**** Build of configuration Debug for project msp430FR5994_IBC_04SH ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O
Building file: "../CLoraModule.cpp"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/ti-cgt-msp430_18.9.0.STS/bin/cl430" -vmspx --code_model=large --data_model=restricted --near_data=none -Ooff --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Projekte/msp430/workspace_v8_x_shaag/msp430FR5994_IBC_04SH" --include_path="C:/Projekte/msp430/workspace_v8_x_shaag/msp430FR5994_IBC_04SH/driverlib/MSP430FR5xx_6xx" --include_path="C:/ti/ccsv8/tools/compiler/ti-cgt-msp430_18.9.0.STS/include" --advice:power=all --advice:hw_config=all --define=__MSP430FR5994__ --define=_MPU_ENABLE -g --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --preproc_with_compile --preproc_dependency="CLoraModule.d_raw" "../CLoraModule.cpp"
>> Compilation failure
subdir_rules.mk:128: recipe for target 'CLoraModule.obj' failed
"../CLoraModule.cpp", line 50: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 139: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 141: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 151: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 152: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 156: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 157: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 158: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 141: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 190: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 192: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 202: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 203: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 207: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 208: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 209: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 192: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 283: remark #1528-D: (ULP 3.1) Detected flag polling using EUSCI_A_UART_BUSY. Recommend using an interrupt combined with enter LPMx and ISR
"../CLoraModule.cpp", line 274: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 276: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 338: remark #1528-D: (ULP 3.1) Detected flag polling using EUSCI_A_UART_BUSY. Recommend using an interrupt combined with enter LPMx and ISR
"../CLoraModule.cpp", line 326: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 331: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 333: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 335: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 365: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 367: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 369: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 394: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 422: remark #2553-D: (ULP 14.1) Array index (involving "i") of type "int". Recommend using "unsigned int"
"../CLoraModule.cpp", line 588: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 718: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 719: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 723: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 724: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 725: remark #1530-D: (ULP 5.1) Detected modulo operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 892: remark #1530-D: (ULP 5.1) Detected divide operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive
"../CLoraModule.cpp", line 894: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 894: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 1238: remark #1528-D: (ULP 3.1) Detected flag polling using EUSCI_A_UART_BUSY. Recommend using an interrupt combined with enter LPMx and ISR
"../CLoraModule.cpp", line 1194: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../CLoraModule.cpp", line 1195: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../CLoraModule.cpp", line 1211: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
INTERNAL ERROR: C:\ti\ccsv8\tools\compiler\ti-cgt-msp430_18.9.0.STS\bin\acpia430.exe experienced a segmentation fault
while processing function (unknown or file scope) file ../CLoraModule.cpp line 1249
This is caused by a defect in the TI EABI C/C++ Parser.
TI Customer Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue".
We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment
gmake: *** [CLoraModule.obj] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
Unfortunately I can´t share the project, but do you have any idea what could cause this error?