This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28022: Hotkey to change project properties

Part Number: TMS320F28022


Tool/software: Code Composer Studio

Sometimes I want to set the project properties to not erase/program the FLASH.

I do this by menu commands Project->properties->Debug->F28022 Flash Settings then under Flash Program Settings, I pick "Load RAM only"

Of course, sometimes I do want to burn the FLASH.

Is there a way I can...

1) make a hot key (as in Window->preferences->general->Keys)

or maybe better yet

2) make an icon on the tool bar to change this setting.

Thanks, Mark.