Part Number: TMS320C5517
Tool/software: TI C/C++ Compiler
Hi. I'm jeongtae from south korea.
I'm using the TMS320C5517 EVM board.
My problem is that if i use the snprintf or sprintf function, it stop the code operation.
I read about this snprintf sprintf issues in TI forum, i changed the stack and heap size as 1024 and 3072.
However it also did't work.
I test some case.
First, if i make a new project for sprintf or snprintf function, it naturally work fine.
Second, if i worked without sprintf or snprintf function in my code, it also work fine.
Third, if i used another variable type(int, float), every type did't work.
What is wrong?..