every packets are successfully sent and received
what's the problem in ccs?
i launch examplecode, rfpacketTx
and error occured like below:
Cortex_M4_0: Error: (Error -1170 @ 0x0) DAP could not be accessed. Reset the device and try the operation again. If the error persists, check the configuration, power cycle the board, and try to make JTAG settings more stable (for example, lower TCLK). (Emulation package 8.0.803.0)
Cortex_M4_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device and try the operation again. If the error persists, check the configuration, power cycle the board, and try to make JTAG settings more stable (for example, lower TCLK). (Emulation package 8.0.803.0)
........
........
Cortex_M4_0: Could not check target status after 20 attempts.
Cortex_M4_0: Failed to remove debug state from target before disconnect. There may still be a breakpoint op code embedded in program memory. It is recommended that you reset the emulator before connecting and reloading the program before proceeding with debugging
ii's impossible to reset system also
i use this device