Hello,
I am trying to calculate the flash checksum in CCSv4 using the On-Chip Flash tool (menu: tools\On-Chip Flash, then click on the "Calculate Checksum" button), how ever after a long pause I get the following error messages:
C28xx: Calculating checksum...
C28xx: Flash Programmer: Error calculating checksum. Device is locked or not connected. Operation cancelled.
C28xx: Error: Error 0x80000004/-1044 Fatal Error during: Register, Device driver: Cannot acquire emulator process Possible conflict for device driver usage
I am using a TSM320F2812 DSP, it is connected to the debugger and flash has been loaded with code. In all other respects the debugger works OK. The JTAG port from the F2812 is connected straight through to a Blackhawk USB510L JTAG Emulator. There are no pull up resisitors on the lines and no buffering (the JTAG connector is within an inch of the F2812 pins).
Running CCSv4 Version 4.2.0.10017.
If anyone has any thoughts, please let me know.
Thanks,
Ian.