Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: CC2640R2F, C2000WARE, CC1310
Tool/software: Code Composer Studio
I contacted Ti with the following questions. They suggested posting on this forum.
I have a few questions about the LAUNCHXL-CC2640R2.
I’m looking at applications where I think the CC2640R2F would fit.
I’ve worked with other programming/microprocessors in the past (more Atmel based).
I downloaded Code Composer Studio (CCS), and was trying to “test-drive” it a little.
I think it could be inexperience on my part, but CCS didn’t seem to auto-complete well, or have good intellisense. When I type in a function, it seemed to recognize it was a function (would auto insert an open parenthesis), but did not offer help on what arguments should be passed to the function. I also does not seem to have intellisense.
I’m kind-of spoiled using visual studio (and similar IDEs), and was wondering if there is a better IDE. Perhaps I’m not experienced enough with CCS, or there is a better IDE I should try. I’ve used visual-studio based IDEs for other processors, and thought maybe TI had one.
I would like to avoid cloud-based IDEs (I’d like the IDE to run on my local CPU). This is due to the fact sometimes I need to work completely off the network. If needed, I could use a cloud-based IDE, but I think you see the challenges.
Thanks for any thoughts.