Part Number: CC2642R
Tool/software: Code Composer Studio
I urgently need your help. I am totally new for TI CCS programming and I am currently developing SPI communication from the SDK example of SPI_Master. In the example the SPI_MASTER uses three pins for MOSI,MISO and Clock. So, for the CS I want to use one pin to be controlled by the software and I used "Board_SPI_MASTER_READY" which is DIO-15. Observing on the output it seems that the master write is working but I am not getting any response from the slave device which is FM25V05-G. Here I have attached my code.
/*
* Copyright (c) 2015-2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== empty.c ========
*/
/* For usleep() */
#include <unistd.h>
#include <stdint.h>
#include <stddef.h>
#include <string.h>
#include <time.h>
#include <pthread.h>
/* Driver Header files */
#include <ti/drivers/GPIO.h>
// #include <ti/drivers/I2C.h>
// #include <ti/drivers/SDSPI.h>
#include <ti/drivers/SPI.h>
// #include <ti/drivers/UART.h>
// #include <ti/drivers/Watchdog.h>
/* Board Header file */
#include "Board.h"
/* FRAM OPCODES*/
#define WREN 0x06 // Write Enable Opcode
#define WRIDI 0x04 // Write Disable Opcode
#define RDSR 0x05 // Read Status Register Opcode
#define WRSR 0x01 // Write Status Register Opcode
#define READ 0x03 // Read Opcode
#define WRITE 0x02 // Write Opcode
#define FSTRD 0x0B // Fast Read Opcode
#define SlEEP 0xB9 // Enter Sleep Mode
#define RDID 0x9F // Read Device ID
SPI_Handle spi;
SPI_Transaction spiTransaction;
SPI_Params spiParams;
void FM25L512_Write_En(uint8_t Opcode1)
{
uint8_t transmitBuffer[1];
uint8_t receiveBuffer[1];
memset(transmitBuffer,0,sizeof(transmitBuffer));
memset(receiveBuffer,0,sizeof(receiveBuffer));
transmitBuffer[0] = Opcode1;
spiTransaction.count = sizeof(transmitBuffer);
spiTransaction.txBuf = (void *)transmitBuffer;
spiTransaction.rxBuf = (void *)receiveBuffer;
SPI_transfer(spi, &spiTransaction);
}
void FM25L512_Write_SPI( uint8_t Opcode1, uint8_t MSBAddr,uint8_t LSBAddr, uint8_t Data)
{
uint8_t transmitBuffer[4];
uint8_t receiveBuffer[4] ;
memset(transmitBuffer,0,sizeof(transmitBuffer));
memset(receiveBuffer,0,sizeof(receiveBuffer));
transmitBuffer[0] = Opcode1;
transmitBuffer[1] = MSBAddr;
transmitBuffer[2] = LSBAddr;
transmitBuffer[3] = Data;
spiTransaction.count = sizeof(transmitBuffer);
spiTransaction.txBuf = (void *)transmitBuffer;
spiTransaction.rxBuf = (void *)receiveBuffer;
SPI_transfer(spi, &spiTransaction);
}
uint8_t FM25L512_SPI_Read(uint8_t Opcode1, uint8_t MSBAddr,uint8_t LSBAddr)
{
uint8_t transmitBuffer[4];
uint8_t receiveBuffer[4];
uint8_t SReadMsg = 0x00;
memset(transmitBuffer,0,sizeof(transmitBuffer));
memset(receiveBuffer,0,sizeof(receiveBuffer));
transmitBuffer[0] = Opcode1;
transmitBuffer[1] = MSBAddr;
transmitBuffer[2] = LSBAddr;
spiTransaction.count = sizeof(transmitBuffer);
spiTransaction.txBuf = (void *)transmitBuffer;
spiTransaction.rxBuf = (void *)receiveBuffer;
SPI_transfer(spi, &spiTransaction);
SReadMsg = receiveBuffer[3];
return SReadMsg;
}
uint8_t FM25L512_Read_SR(uint8_t Opcode)
{
uint8_t transmitBuffer[2];
uint8_t receiveBuffer[2];
uint8_t SRMsg = 0x00;
memset(transmitBuffer,0,sizeof(transmitBuffer));
memset(receiveBuffer,0,sizeof(receiveBuffer));
transmitBuffer[0] = Opcode;
spiTransaction.count = sizeof(transmitBuffer);
spiTransaction.txBuf = (void *)transmitBuffer;
spiTransaction.rxBuf = (void *)receiveBuffer;
SPI_transfer(spi, &spiTransaction);
SRMsg = receiveBuffer[1];
return SRMsg;
}
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
// GPIO initialization
GPIO_init();
GPIO_setConfig(Board_SPI_MASTER_READY, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_HIGH);
GPIO_write(Board_SPI_MASTER_READY, 1);
/* Call driver init functions */
SPI_init();
/* Configure the LED pin */
GPIO_setConfig(Board_GPIO_LED0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
/* Turn on user LED */
GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON);
SPI_Params_init(&spiParams); // Initialize SPI parameters
spiParams.dataSize = 8; // 8-bit data size
spi = SPI_open(Board_SPI0, &spiParams);
if (spi == NULL) {
while (1); // SPI_open() failed
}
// SPI Transaction with CS
// Write Enable
GPIO_write(Board_SPI_MASTER_READY, 0);
__delay_cycles(0.05);// Delay for the CS to get ready
FM25L512_Write_En(WREN);
GPIO_write(Board_SPI_MASTER_READY, 1);
__delay_cycles(10);
// Data Write
GPIO_write(Board_SPI_MASTER_READY, 0);
__delay_cycles(0.05);
FM25L512_Write_SPI(WRITE,0x00,0x00,0x07);
__delay_cycles(0.05);
GPIO_write(Board_SPI_MASTER_READY, 1);
__delay_cycles(10);
// Data Read
__delay_cycles(10);
GPIO_write(Board_SPI_MASTER_READY, 0);
__delay_cycles(100);
FM25L512_SPI_Read(READ,0x00,0x00);
__delay_cycles(10);
GPIO_write(Board_SPI_MASTER_READY, 1);
__delay_cycles(10);
while (1) {
usleep(100000);
GPIO_toggle(Board_GPIO_LED0);
}
}