Part Number: CCSTUDIO
Tool/software: TI C/C++ Compiler
Hi, there. As title, How to compile one single source file?
I only found a option "Build Selected File(s)", but didn't response anything after clicking it.
I want to compile file sockets.c, but nothing happened after clicking it.
Why I want to compile sockets.c? Because I found a weird thing.
At second image, I can't locate right bracket of function lwip_sendto by right clicking left bracket of it.
I started to debug this function and found that there is a superfluous left bracket at line 40.(Could line number show up before posting?)
int
lwip_sendto(int s, const void *data, size_t size, int flags,
const struct sockaddr *to, socklen_t tolen)
{
struct lwip_sock *sock;
err_t err;
u16_t short_size;
const struct sockaddr_in *to_in;
u16_t remote_port;
#if !LWIP_TCPIP_CORE_LOCKING
struct netbuf buf;
#endif
sock = get_socket(s);
if (!sock) {
return -1;
}
if (sock->conn->type == NETCONN_TCP) {
#if LWIP_TCP
return lwip_send(s, data, size, flags);
#else /* LWIP_TCP */
LWIP_UNUSED_ARG(flags);
sock_set_errno(sock, err_to_errno(ERR_ARG));
return -1;
#endif /* LWIP_TCP */
}
/* @todo: split into multiple sendto's? */
LWIP_ASSERT("lwip_sendto: size must fit in u16_t", size <= 0xffff);
short_size = (u16_t)size;
LWIP_ERROR("lwip_sendto: invalid address", (((to == NULL) && (tolen == 0)) ||
((tolen == sizeof(struct sockaddr_in)) &&
((to->sa_family) == AF_INET) && ((((mem_ptr_t)to) % 4) == 0))),
sock_set_errno(sock, err_to_errno(ERR_ARG)); return -1;);
to_in = (const struct sockaddr_in *)(void*)to;
#if LWIP_TCPIP_CORE_LOCKING
/* Should only be consider like a sample or a simple way to experiment this option (no check of "to" field...) */
{
struct pbuf* p;
ip_addr_t *remote_addr;
#if LWIP_NETIF_TX_SINGLE_PBUF
p = pbuf_alloc(PBUF_TRANSPORT, short_size, PBUF_RAM);
if (p != NULL) {
#if LWIP_CHECKSUM_ON_COPY
u16_t chksum = 0;
if (sock->conn->type != NETCONN_RAW) {
chksum = LWIP_CHKSUM_COPY(p->payload, data, short_size);
} else
#endif /* LWIP_CHECKSUM_ON_COPY */
MEMCPY(p->payload, data, size);
#else /* LWIP_NETIF_TX_SINGLE_PBUF */
p = pbuf_alloc(PBUF_TRANSPORT, short_size, PBUF_REF);
if (p != NULL) {
p->payload = (void*)data;
#endif /* LWIP_NETIF_TX_SINGLE_PBUF */
if (to_in != NULL) {
inet_addr_to_ipaddr_p(remote_addr, &to_in->sin_addr);
remote_port = ntohs(to_in->sin_port);
} else {
remote_addr = &sock->conn->pcb.raw->remote_ip;
if (sock->conn->type == NETCONN_RAW) {
remote_port = 0;
} else {
remote_port = sock->conn->pcb.udp->remote_port;
}
}
LOCK_TCPIP_CORE();
if (sock->conn->type == NETCONN_RAW) {
err = sock->conn->last_err = raw_sendto(sock->conn->pcb.raw, p, remote_addr);
} else {
#if LWIP_UDP
#if LWIP_CHECKSUM_ON_COPY && LWIP_NETIF_TX_SINGLE_PBUF
err = sock->conn->last_err = udp_sendto_chksum(sock->conn->pcb.udp, p,
remote_addr, remote_port, 1, chksum);
#else /* LWIP_CHECKSUM_ON_COPY && LWIP_NETIF_TX_SINGLE_PBUF */
err = sock->conn->last_err = udp_sendto(sock->conn->pcb.udp, p,
remote_addr, remote_port);
#endif /* LWIP_CHECKSUM_ON_COPY && LWIP_NETIF_TX_SINGLE_PBUF */
#else /* LWIP_UDP */
err = ERR_ARG;
#endif /* LWIP_UDP */
}
UNLOCK_TCPIP_CORE();
pbuf_free(p);
} else {
err = ERR_MEM;
}
}
#else /* LWIP_TCPIP_CORE_LOCKING */
/* initialize a buffer */
buf.p = buf.ptr = NULL;
#if LWIP_CHECKSUM_ON_COPY
buf.flags = 0;
#endif /* LWIP_CHECKSUM_ON_COPY */
if (to) {
inet_addr_to_ipaddr(&buf.addr, &to_in->sin_addr);
remote_port = ntohs(to_in->sin_port);
netbuf_fromport(&buf) = remote_port;
} else {
remote_port = 0;
ip_addr_set_any(&buf.addr);
netbuf_fromport(&buf) = 0;
}
LWIP_DEBUGF(SOCKETS_DEBUG, ("lwip_sendto(%d, data=%p, short_size=%"U16_F", flags=0x%x to=",
s, data, short_size, flags));
ip_addr_debug_print(SOCKETS_DEBUG, &buf.addr);
LWIP_DEBUGF(SOCKETS_DEBUG, (" port=%"U16_F"\n", remote_port));
/* make the buffer point to the data that should be sent */
#if LWIP_NETIF_TX_SINGLE_PBUF
/* Allocate a new netbuf and copy the data into it. */
if (netbuf_alloc(&buf, short_size) == NULL) {
err = ERR_MEM;
} else {
#if LWIP_CHECKSUM_ON_COPY
if (sock->conn->type != NETCONN_RAW) {
u16_t chksum = LWIP_CHKSUM_COPY(buf.p->payload, data, short_size);
netbuf_set_chksum(&buf, chksum);
err = ERR_OK;
} else
#endif /* LWIP_CHECKSUM_ON_COPY */
{
err = netbuf_take(&buf, data, short_size);
}
}
#else /* LWIP_NETIF_TX_SINGLE_PBUF */
err = netbuf_ref(&buf, data, short_size);
#endif /* LWIP_NETIF_TX_SINGLE_PBUF */
if (err == ERR_OK) {
/* send the data */
err = netconn_send(sock->conn, &buf);
}
/* deallocated the buffer */
netbuf_free(&buf);
#endif /* LWIP_TCPIP_CORE_LOCKING */
sock_set_errno(sock, err_to_errno(err));
return (err == ERR_OK ? short_size : -1);
}
With extra left bracket, I have no idea that why my library(including this sockets.c source file)is compiled successfully.
So I want to standalone this one and compile it.
Thank you.