This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5529: CCS can not build the project and debug

Part Number: MSP430F5529

Tool/software: Code Composer Studio

I have changed some set corresponding the hardware, I don't know why there were many errors when I used Debug. I use CCS ver. 5 to handle with this project because I see the ccs project in SDK is also on version 5. I try many methods from other people had encountered the similar problems and resolve problems on the Internet, but my problem is still not improved. I guess the problem is related to the compiler version because there are different errors when I use different compiler version.  I have installed all compiler version ,but I only see three types

anyway, the result is below

compilier version TI v4.2.1 and TI v4.4.8 have the same result

There is no problem when i use compilier version TI v18.9.0, but I can see it has many fatal errors on CDT Build Console. Then it will show the error message.

If anyone know how to solve this problem, please tell me some solutions,thanks!