This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSK 6713 + CCS V3.3

I board DSK 6713 was purchased with CCS V1. But for some reason i want to use CCS V3.3. I have found that previous driver will not work. So i have downloaded the driver from the site http://support.spectrumdigital.com/ccs33/    . After installation the driver  in the CCS SETUP  it is showing the option to select DSK 6713 (big & Little). I have selected it. Then whenever i am trying to open  the CCS it is showing the following error message .

Unable to find an appropriate registry key for  "TMS320C2XX"                                                                                                                                                                                                                  Target driver: C:\CCSudio_v3.3\drivers\sdgo6713dsk.dvr

Please help me to fix this error.

Regards

Biprangshu Saha

 

 

  • Biprangshu,

    Where did you get your CCS installation?  I believe you are using a build of CCSv3.3 that does not support the device you are trying to use.  Most of the versions of CCSv3.3 that are bundled with a particular development kit will only work with that kit and cannot be used with a different board.

    Regards,

    John

     

  • I recommend using CCS 4.  You can always get the latest and greatest free for use with EVMs and all the drivers come built into it.

  • Thanx John & Brad.

    Its a great idea to use CCS4. I have tried to use the CCS4. But getting some prolem connecting the device.

    1.I am not able to understand which connection type shold i use (like i. Bjackhawk USB2.0 Emulator     ii. Spectrum digital DSK-EVM -eZDSP onboard USB  Emulator   etc). Both & many other connection type showing the same device.

    2. What will bhe the sequence of operation to connect to connect the device -  Spectrum digotal TMS320C6713 DSK,   in CCS4

    if any link is available plz post it .

  • Thanx a lot.

    One last & most important thing to be asked.

    1.will the same code made for DSK6713 + CCS 3.1,  run in DSK6713+ CCs4

    2. What will be the proper sequence of operation to make a project, is that same as CCS 3.1

    3. With CCS 3.1 cd I got  a tutorial of DSK 6713  with following contents

    i) Development Environment

     ii)Loading & running a program

    iii) introduction to DSP bias

    iv) BSL overview

    v) BSL API  list with description

    Vi) Different examples in CCS3.1 environment

    etc

    From where can I get  the same for CCS4 to work on DSK 6713

     

    4. Also i am not finding any DSK 6713 specific files like include file, .lib, .hlp files etc , in  Texus Instrument folder.

    5. Can  u post  any link regarding examples for c6713+ccsv4

    In a word it will be very helpful if i get proper tutorial for DSK 6713 + CCS$

  • Thanx a lot.

    One last & most important thing to be asked.

    1.will the same code made for DSK6713 + CCS 3.1,  run in DSK6713+ CCs4

    2. What will be the proper sequence of operation to make a project, is that same as CCS 3.1

    3. With CCS 3.1 cd I got  a tutorial of DSK 6713  with following contents

    i) Development Environment

     ii)Loading & running a program

    iii) introduction to DSP bias

    iv) BSL overview

    v) BSL API  list with description

    Vi) Different examples in CCS3.1 environment

    etc

    From where can I get  the same for CCS4 to work on DSK 6713

     

    4. Also i am not finding any DSK 6713 specific files like include file, .lib, .hlp files etc , in  Texus Instrument folder.

    5. Can  u post  any link regarding examples for c6713+ccsv4

    In a word it will be very helpful if i get proper tutorial for DSK 6713 + CCS4

  • Biprangshu Saha said:
    1.will the same code made for DSK6713 + CCS 3.1,  run in DSK6713+ CCs4

    Correct.  The code should not have to change.

     

    Biprangshu Saha said:
    2. What will be the proper sequence of operation to make a project, is that same as CCS 3.1

    http://processors.wiki.ti.com/index.php/CCSv4_Getting_Started_Guide

     

    Biprangshu Saha said:

    3. With CCS 3.1 cd I got  a tutorial of DSK 6713  with following contents

    i) Development Environment

     ii)Loading & running a program

    iii) introduction to DSP bias

    iv) BSL overview

    v) BSL API  list with description

    Vi) Different examples in CCS3.1 environment

    etc

    From where can I get  the same for CCS4 to work on DSK 6713

    We expect you to import the project into CCS 4

     

    Biprangshu Saha said:
    4. Also i am not finding any DSK 6713 specific files like include file, .lib, .hlp files etc , in  Texus Instrument folder.

    .

    You can use all your existing library files in CCS 4.  The BSL, etc are owned by the board manufacturer, Spectrum Digital.

     

    Biprangshu Saha said:

    5. Can  u post  any link regarding examples for c6713+ccsv4

    In a word it will be very helpful if i get proper tutorial for DSK 6713 + CCS4

    Given the age of the 6713 you should not count on seeing any such tutorials from TI.  You might instead take a look at the Integration Workshop Using DSP/BIOS.  The current version is made to work with the C6748 DSP (2 generations past the 6713) and it has many labs and step-by-step instructions that sound more like what you are looking for.  The OMAPL138 Experimenter Kit is a relatively low cost way to get access to this board.