This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: CCSv8.2 install

Part Number: CODECOMPOSER

Tool/software: Code Composer Studio

Hi, 

I got a problem on installing CCS v8.2 in a SUSE linux 64bit server. 

 

I downloaded the v8.2 offline installer. When I enter ./ccs_setup.bin, it shows nothing. I tried both sudo and not. It did not work. And I can't find any relevant file after unpacking. Following is the install log.

Hope you guys can give me some helps.

Thank you in advance,

Rui

  • Hi Rui,

    Could you please attach that log here?

    Thanks,

    Danish

  • That's all I got.
    --------------------------------------------------

    vim ccs_8.2.0.00007.log
    Log started 12/06/2018 at 14:49:47
    Preferred installation mode : unattended
    Trying to init installer in mode unattended
    Mode unattended successfully initialized
    [14:49:47] Found mode
    [14:49:47] Suse
    [14:49:47] installer_command_line_arguments :

    [14:49:47] installer_command_line_arguments :
    [14:49:48] Product Name Code Composer Studio 8.2.0
    [14:49:48] Product Version 8.2.0.00007
    [14:49:48]
    Preparing to Install
    Preparing to Install
    Unpacking files
    Unpacking files
    Unpacking files
    Unpacking files
    Unpacking files
    Unpacking files
    Unpacking files
    [14:49:48] admin = 1
    [14:49:48] installertype = setup
    [14:49:48] ccsinstaller_name ccs_setup_linux64_8.2.0.00007.bin
    [14:49:48] Installer: /usr/local/share/CCS8.2.0.00007_linux-x64/ccs_setup_linux64_8.2.0.00007.bin
    Executing chmod -R 777 "/tmp/ccs_4dc0ef71-a690-4897-691e-d0d88cfa3c73/tcl"
    Script exit code: 0

    Script output:


    Script stderr:


    Executing chmod -R 777 "/tmp/ccs_4dc0ef71-a690-4897-691e-d0d88cfa3c73/util"
    Script exit code: 0

    Script output:

    "ccs_8.2.0.00007.log" 128L, 4949C
  • rui zhang43 said:
    I got a problem on installing CCS v8.2 in a SUSE linux 64bit server. 

    Unfortunately, SUSE is not one of our tested environments, so we are currently unable to reproduce or validate the errors you are reporting. 

    Please try to install and use the product on one of the supported Linux hosts

  • Is there any version after v3.3 support SUSE?
    Thanks
  • Sorry, no. That is not an environment we have validated/supported any of our CCS versions with.