This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5994: New debugger MSP-FET. slow and causes extra wakes from LPM in debug mode

Part Number: MSP430FR5994
Other Parts Discussed in Thread: MSP-FET

Tool/software: Code Composer Studio

Hi folks, 

i've just upgraded my MSP-FET430UIF to the newer MSP-FET.   i just plugged it in and started using with CCS. 

It works, but seems slow. I'm using the backchannel uart at 19200baud, and this seems really sluggish (very noticeable lag between typing on the pc and getting echo'd back / processed by the msp).

Also, during debugging, it is causing two runs round my main loop, for every one wake from interrupt. i've confirmed this doesn't happen with the old FETUIF debugger, and doesn't happen when running standalone. 

When using the older FETUIF, im using an FTDI serial cable with otherwise the same setup, and it is quick to respond, with no issues. 

Should i be using a newer / different driver for the MSP-FET? 

Thanks,

Michael.