This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4 Logging Error

Other Parts Discussed in Thread: DA8XX

If RTA Raw Logs are enabled when running my application (on the DA8XX EVM) , the log window closes with the following error.

eclipse.buildId=4.1.0.02006
java.version=1.5.0_14
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Command-line arguments:  -os win32 -ws win32 -arch x86

Error
Thu Nov 25 14:57:55 IST 2010
-8
Plug-in

com.ti.dvt.rta.xdc.dp.XDCLogSource$DSThread

 

After this CCS hangs and I need to restart it. This is really hampering the debugging. Is there anyway I can get some more information regarding this ?

Regards and Thanks,

Maya Kamath.