This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/F28M36P63C2: XDS100V2 Emulator test connection fail



Tool/software: Code Composer Studio

Hello all,

I have been trying to connect to my custom made F28M36 board and when i set the adaptive clocking frequency and test the connection, i get the following error message

This error is generated by TI's USCIF driver or utilities.

The value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.

The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.

[End: Texas Instruments XDS100v2 USB Debug Probe_0]

I verified while using MPROG to load the correct .ept file into EEPROM, that i have VID=0403 PID=A6D0. What could cause this error?

Thanks,

Srini