Part Number: CC3200
Other Parts Discussed in Thread: ADS1247, , ADS1248
Tool/software: Code Composer Studio
Hi
I am interfacing cc3200 with ADS1247 using spi communication.The problem is i am not getting the data.I have checked in oscilloscope that sclk pin is not working means the clk pulse is not coming it is coming as a straight line.And also sometimes the return function of SPIDataPutNonBLocking funtion as 1 and someother time it is giving as 0.Plz help me in resolving the issue.Below i have attached my code.
#include <string.h>
#include "stdbool.h"
#include "stdint.h"
// Driverlib includes
#include "hw_types.h"
#include "hw_memmap.h"
#include "hw_common_reg.h"
#include "hw_ints.h"
#include "spi.h"
#include "rom.h"
#include "rom_map.h"
#include "utils.h"
#include "prcm.h"
#include "uart.h"
#include "interrupt.h"
#include "gpio.h"
#include "pin.h"
// Common interface include
#include "uart_if.h"
#include "ibp.h"
#define SPI_IF_BIT_RATE 1000000
void spiInit();
void IbpInit();
void IBP_initialize();
void send_data(unsigned char );
void rec_data();
//void receive_data1(int );
//bool ibp_self_test();
void main()
{
unsigned char ulUserData[4]="kkll";
unsigned char data4;
unsigned long pui32DataRx[2];
int i=0;
ClearTerm();
InitTerm();
MAP_PRCMPeripheralReset(PRCM_GSPI);
PinMuxConfig();
spiInit();
IbpInit();
// ibp_self_test();
Message("\t\t*************MAIN*******\n\r");
MAP_UARTCharPut(UARTA0_BASE,'c');
for(i=0;i<5;i++)
{
MAP_UARTCharPut(UARTA0_BASE, ulUserData[i]);
}
Message("\t\t*************IBP DATA*******\n\r");
send_data(ADS1248_CMD_ID);
send_data(ADS1248_CMD_WAKEUP);
receive_data(2);
data4= SPIDataGetNonBlocking(GSPI_BASE,&(pui32DataRx[0]));
Report("%x\n",pui32DataRx[0]);
Report("%x\n",&pui32DataRx[0]);
Report("%x\n",data4);
MAP_SPICSDisable(GSPI_BASE);
while(1)
{
// Message("\t\t*************IBP DATA*******\n\r");
//receive_data1(1);
}
}
void IbpInit()
{
// PK2 = POWER CONTROL
MAP_PRCMPeripheralClkEnable(PRCM_GPIOA1, PRCM_RUN_MODE_CLK);
MAP_PinTypeGPIO(PIN_03, PIN_MODE_0,false);
MAP_GPIODirModeSet(GPIOA1_BASE, 0x10, GPIO_DIR_MODE_OUT);
//PK4 = GROUND CONTROL
MAP_PinTypeGPIO(PIN_04, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA1_BASE, 0x20, GPIO_DIR_MODE_OUT);
// PN0 = SPI_EN
MAP_PRCMPeripheralClkEnable(PRCM_GPIOA0, PRCM_RUN_MODE_CLK);
MAP_PinTypeGPIO(PIN_60, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA0_BASE, 0x20, GPIO_DIR_MODE_OUT);
// PN1 = MUX_EN
MAP_PinTypeGPIO(PIN_61, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA0_BASE, 0x40, GPIO_DIR_MODE_OUT);
// PN2 MUX_SELA
MAP_PinTypeGPIO(PIN_62, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA0_BASE, 0x80, GPIO_DIR_MODE_OUT);
// PN3 MUX_sELB
MAP_PinTypeGPIO(PIN_15, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA2_BASE, 0x6, GPIO_DIR_MODE_OUT);
GPIOPinWrite(GPIOA1_BASE,GPIO_PIN_4, GPIO_PIN_4); //PK2=1
GPIOPinWrite(GPIOA1_BASE,GPIO_PIN_5,0); //PK4=1
GPIOPinWrite(GPIOA0_BASE,GPIO_PIN_5,GPIO_PIN_5); //PN0=1
GPIOPinWrite(GPIOA0_BASE,GPIO_PIN_6,GPIO_PIN_6); //PN1=1
GPIOPinWrite(GPIOA0_BASE,GPIO_PIN_7,0); //PN2=0 // mux sel-a
GPIOPinWrite(GPIOA2_BASE,GPIO_PIN_6,0); //PN3=1 // mux sel-b
/* MAP_PRCMPeripheralClkEnable(PRCM_GPIOA2, PRCM_RUN_MODE_CLK);
MAP_PinTypeGPIO(PIN_08, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA2_BASE, 0x2, GPIO_DIR_MODE_OUT);
GPIOPinWrite(GPIOA2_BASE,GPIO_PIN_1,0);*/
MAP_UtilsDelay(100000); //1MS
IBP_initialize(); // in ibp.c
Message("\t\t*******IBPINIT*********\n\r");
}
void spiInit()
{
MAP_PRCMPeripheralClkEnable(PRCM_GSPI, PRCM_RUN_MODE_CLK);
// Configure PIN_05 for SPI0 GSPI_CLK
//
MAP_PinTypeSPI(PIN_05, PIN_MODE_7);
//
// Configure PIN_06 for SPI0 GSPI_MISO
//
MAP_PinTypeSPI(PIN_06, PIN_MODE_7);
//
// Configure PIN_07 for SPI0 GSPI_MOSI
//
MAP_PinTypeSPI(PIN_07, PIN_MODE_7);
//
// Configure PIN_08 for SPI0 GSPI_CS
//
MAP_PinTypeSPI(PIN_08, PIN_MODE_7);
SPIReset(GSPI_BASE);
// Configure SPI interface
//
MAP_SPIConfigSetExpClk(GSPI_BASE,MAP_PRCMPeripheralClockGet(PRCM_GSPI),
SPI_IF_BIT_RATE,SPI_MODE_MASTER,SPI_SUB_MODE_1,
(SPI_SW_CTRL_CS |
SPI_4PIN_MODE |
SPI_TURBO_OFF |
SPI_CS_ACTIVEHIGH|
SPI_WL_8));
Message("\t\t*************SPIINIT*******\n\r");
// Enable SPI for communication
//
MAP_SPIEnable(GSPI_BASE);
MAP_SPICSEnable(GSPI_BASE);
}
/*************************************************************
* Function: IBP_initialize()
*
* Description: This function is called from Main.c before the scheduling function and
* before the self test. This is called after initializng IBP board(mux,speed,etc)
* This is used to initilaize the registers of ADC required for operation of IBP board
* and doing internal adc calibration.
*
* Parameters: NULL
*
* Returns: NULL
*
* Reentrancy: No
*
* Execution Requirements/Assumptions: NULL
*
*************************************************************/
void IBP_initialize()
{
unsigned long pui32DataRx[NUM_SSI_DATA];
while(SPIDataGetNonBlocking(GSPI_BASE, &pui32DataRx[0]))
{
}
//SysCtlDelay(650000); //= 17ms.
//SysCtlDelay(50000);
MAP_UtilsDelay(650000);
MAP_UtilsDelay(50000);
send_data(ADS1248_CMD_RESET);
//SysCtlDelay(50000);
MAP_UtilsDelay(50000);
Message("\t\t*************IBP one*******\n\r");
send_data(ADS1248_CMD_SDATAC);
send_data(ADS1248_CMD_SELFOCAL);
receive_data(1);
//SysCtlDelay(6500000); //17ms
MAP_UtilsDelay(6500000);
send_data(ADS1248_CMD_WREG); //40h
send_data(ADS1248_3_SYS0); //03h
send_data(ADS1248_1_VBIAS); //01h
send_data(ADS1248_0_MUX0); //00h
send_data(ADS1248_2_MUX1); //03h
//send_data(ADS1248_14_GAIN); //42h ADS1248_14_SPS
send_data(ADS1248_15_SPS); // from 5sps(above) to 1000sps it is set. currently set at 160(or something) sps.
receive_data(8);
send_data(ADS1248_CMD_RREG); //20h
send_data(ADS1248_3_SYS0); //03h
receive_data(2);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_SYSGCAL);
receive_data(1);
//SysCtlDelay(6500000); //17ms
MAP_UtilsDelay(650000);
//14-----Write the respective register configuration with the WREG command (40h, 03h, 01h, 00h, 03h and 42h); --pg 37 datasheet
send_data(ADS1248_CMD_WREG); //40h
send_data(ADS1248_3_SYS0); //03h
send_data(ADS1248_1_VBIAS); //01h
send_data(ADS1248_0_MUX0); //00h
send_data(ADS1248_0_MUX0); //03h
send_data(ADS1248_15_SPS); //42h
receive_data(6);
send_data(ADS1248_CMD_RREG); //20h
send_data(ADS1248_3_SYS0);
receive_data(2);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_NOP);
receive_data(1);
send_data(ADS1248_CMD_SYNC); //05h
send_data(ADS1248_CMD_SYNC); //05h-------////because we have to give sync command twice---pg 38
receive_data(2);
//SysCtlDelay(650000);
MAP_UtilsDelay(650000);
Message("\t\t*************LAST IBP INIT*******\n\r");
}
void send_data(unsigned char Byte)
{
unsigned char data;
data=SPIDataPutNonBlocking(GSPI_BASE,Byte);
Report("\t\tsend data=%d\n\r",data);
}
void receive_data(int n)
{
unsigned long rec=0;
unsigned char data=0;
data=SPIDataGetNonBlocking(GSPI_BASE,&rec);
Report("\t\trec1= %d\n\r",rec);
Report("\t\t rec=%d\n\r",data);
}