Part Number: TMS320C5515
Tool/software: Code Composer Studio
Hi,
We have a set of legacy projects which were created in Code Composer Studio v3.3.
We are currently using Code Composer Studio v8.2.
We run into situations where we have to import the old projects into the newer version of Code Composer Studio from time to time.
Once the projects are imported into CCS v8.2 we have to do a moderate amount of work to the project settings in order to get the project operational and compiling properly.
Is there a way in CCS v8.2 to export the project in CCS v8.2 format so that in the future should we need to import the project on another computer it can be done so as a CCS v8.2 project and not CCS v3.3 project?
This would hopefully eliminate the process of modifying the project settings after the project was imported.
Thanks