Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Resharing a probable bug found in CCSv8.3.0 from the below thread upon request. (below if the link for the original thread).
Hi TIers,
I am running test programs from BSL (board Support libraries) for TMS320C5505 eZDSP USB stick and I keep getting the below Internal Stack overflow Error when I try to build the project. (Nothing extra other than building the project is running while trying to build the project).
Environment: Win 10+ DSP BIOSv5.42.2.10 + CCSv8.3.0
Code Compiler: BSL is configured to use C5500 (TI v4.3.2) but is using TIv4.4.1 as this is the only C5500 compiler version installed on the PC.
Any help would be appreciated to resolve this. Please suggest. Thank you. in advance for your time and patience.
Solution: This is a possible bug. I did install an earlier version and didn't face this issue with earlier version of CCS (v8.1.0). Hope this helps.