This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6713B: TMS320C6713 DSK kit with the CCS V7.4, It showing that device drivers are not installed.

Part Number: TMS320C6713B


Tool/software: Code Composer Studio

Hello,

This is the reply last time suggested by TI employee, 

You need to install CCS with Spectrum Digital driver support. While it comes bundled with the CCS installer, it is not installed by default when you install CCS. You need to explicitly enable it. If you did not install it, you can re-run the CCS installer over your existing installation. The installer will detect an existing CCS installation and will allow you to add additional components that you missed the first time.

            When I re-run the CCS installer for multiple times, the CCS installer does not detect any device drivers. Kindly resolve my issue.

             PC configuration:

           Windows 7, Intel Core 2 Duo processor