Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK, CC2530, CC2531
Tool/software: Code Composer Studio
Hi,
I want to prototype ZigBee device based on CC2538. I understand CCS supports this chip (there's even an option to download its support during the installation). However I can't find any examples of the Zigbee app for that chip. In fact I can't even find the zstack itself...
I'll appreciate a bit of guidance with regards to setting up the CCS to the point I have an example Zigbee project for CC2538 compiling. I tried IAR too the trial is only 30 days and I can't download z-stack 3.0 for IAR too. Also I'm a linux user so CCS would work much better than IAR for me.
Regards,
Witek