Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: C2000WARE,
Tool/software: Code Composer Studio
Respected Sir,
I was trying to install the CCS 8.3 (latest version) on my PC having windows 8 OS. When the installation gets finished, I have imported one example code from C2000Ware and trying to build it. While building the example code, CCS is giving gmake errors. I thought it is in installation issue, so I have uninstalled it and reinstalled still facing the same errors. I have disabled the Quick heal, and Windows defender while installing.
The second thing is that I have simulated one design in MATLAB which is also not running on that PC for hardware. Embedded coder is giving problem related to CCS. The same Matlab design I have run on another PC
and also run on hardware (LAUNCHXL-F28069M). Embedded coder is generating the code for that simulation. I have imported that code in CCS and debug it, It is running fine with another PC where CCS is installed properly. The another PC is also running the example codes properly. Both PC have same configurations, features, and settings then what will be the problem with 1st PC. I have attached the snapshot of errors kindly find it.
Regards,
Nisha Gosavi