Other Parts Discussed in Thread: CCSTUDIO
I have a problem. I use CCS V3.3 Platinum ( limited 32k) . I open a project ( from internet LF24xx example ), but I can’t compile it .
CSS warns :
" Build error: cannot run dspcl.
Build error: cannot run dspcl.
Build Complete,
2 Errors, 0 Warnings, 0 Remarks"
I found "dspcl" in help. It's "Command that runs the compiler and the assembler" .
I opened the other project ( eg : F2808 or F28035, F28335 examples . It's ok. I can compile them) I don't understand. I think CCS V3.3 support to 24xx because allowing to choose 24xx device when creating a new project.
How to sovle this problem ?