This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS v3.3 installation problem (Error 1721)



Tool/software: Code Composer Studio

Running into an issue on installation of CCS v3.3 setup as i get the following error "Error 1721: There is a problem with the windows installer package.  A program required to complete this install could not be run.  Contact support personnel or vendor"..

I am running windows 10 and have the sufficient admin privileges and space.  

Any help would be appreciated.

  • Hello,
    Most likely there was some component bundled with the installer that was unable to be installed. The most common one is DSP/BIOS.

    Note that CCSv3.3 is not supported on Windows 10. If you must use CCSv3.3, I strongly suggest using Windows XP - which is last version of Windows officially supported. Many people still use CCSv3.3 in a Windows XP VM. Otherwise, please update your CCS version to something more current.

    Thanks
    ki