Part Number: CCSTUDIO
Tool/software: TI C/C++ Compiler
Hi, I'm reading TMS320C6000 Assembly language tools User Guide according to this link: https://e2e.ti.com/support/processors/f/791/t/59430
I'm reading Chapter 2, and it says:
「Several assembler directives allow you to associate various portions of code and data with the appropriate sections.」
I've only written C, and I'm with little experience on reading assembly code.
Q1: I didn't recall any directive in .asm file that I read before. Is dividing file into sections by using directives necessary or depending on Compiler?
I know that C programming language has by nature sections concept, e,g, variables outside any function are global, inside are local, and Compiler can take advantage of this for dividing sections. Therefore there is no need of programmer using directives in C source file.
Q2: Is my conclusion, as to last sentence, correct?
The user guide also says:
「The linker has two main functions related to sections. First, the linker uses the sections in object files as building blocks; it combines input sections (when more than one file is being linked) to create output sections in an executable output module. Second, the linker chooses memory addresses for the output sections.」
「Two linker directives support these functions:
• The MEMORY directive allows you to define the memory map of a target system. You can name portions of memory and specify their starting addresses and their lengths.
• The SECTIONS directive tells the linker how to combine input sections into output sections and where to place these output sections in memory.」
Q3: I didn't see "SECTIONS directive tells the linker how to combine input sections into output sections" in my linker command file.
7.4.9 Define an Entry Point (--entry_point Option) from User Guide
「The memory address at which a program begins executing is called the entry point. When a loader loads a program into target memory , the program counter (PC) must be initialized to the entry point; the PC then points to the beginning of the program. The linker can assign one of four values to the entry point. These values are listed below in the order in which the linker tries to use them. If you use one of the first three values, it must be an external symbol in the symbol table.
• The value specified by the --entry_point option. The syntax is: --entry_point= global_symbol where global_symbol defines the entry point and must be defined as an external symbol of the input files.
• The value of symbol _c_int00 (if present). The _c_int00 symbol must be the entry point if you are linking code produced by the C compiler.
• The value of symbol _main (if present)
• 0 (default value)」
Q4: The Linker options "-e Entry" is not described by user guide.