This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: Problem with sprintf function DSP F28334

Tool/software: TI C/C++ Compiler

Hi ,

I'm having trouble using sprintf function with code composer studio 8 and c compiler v 6.2.11 . I'm tryng to build a string in this way :

sprintf((char *)wifi_info.jsonTxBuffer, "{\"cmdId\":%d,\"quote\":%u,\"speed\":%d,\"state\":%d,\"errorMask\":%d}", CMDGETPDO, sumFir, velMandToTransmit, stateByte, errMask);

but in the result buffer the variables are printed shifted.  For example the correct result will be the string:

{"cmdId":0, "quote":292, "speed":0, "stateByte":0,"errMask":340} 

instead what i get is:

{"cmdId":0, "quote":0, "speed":0, "stateByte":292,"errMask":0}  or sometimes in the second %d character there's a random number.

If i use it with fixed values instead of variables it works fine ( sprintf((char *)wifi_info.jsonTxBuffer, "{\"cmdId\":%d,\"quote\":%u,\"speed\":%d,\"state\":%d,\"errorMask\":%d}", 10, 11, 12, 13, 14); )

I set the stack and heap size , and also enabled  --printf_support=minimal compiler option (stdio.h is also included).

Does anyone experienced the same issue?

Regards.

Fabio