This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: gmake*** error

Part Number: TMS320F28335


Tool/software: Code Composer Studio

I am getting following errors can someone guide me on how to fix them. 

Description Resource Path Location Type
#1965 cannot open source file "PWMConfig.h" projectall.h /Microgrid_BDC/SPWM Include line 45 C/C++ Problem

gmake: *** [flash_src/DSP2833x_Adc.obj] Error 1 Microgrid_BDC C/C++ Problem

gmake: *** [flash_src/DSP2833x_CpuTimers.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_DefaultIsr.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_GlobalVariableDefs.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_Gpio.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_MemCopy.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_PieCtrl.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_PieVect.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_Sci.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [flash_src/DSP2833x_SysCtrl.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/ADCConfig.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/Controler.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/DFilter.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/main_test.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/PQControl.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/PWMConfig.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/SciConfig.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: *** [SPWM Src/SinCos.obj] Error 1 Microgrid_BDC C/C++ Problem
gmake: Target 'all' not remade because of errors. Microgrid_BDC C/C++ Problem

  • Hi,

    The error below indicates which file the C/C++ compiler it can't find, as well as the file that includes it and the line the problem is located.
    #1965 cannot open source file "PWMConfig.h" projectall.h /Microgrid_BDC/SPWM Include line 45 C/C++ Problem

    I strongly suggest you to locate where the missing file is located in your filesystem and add the path to the Compiler include paths of your project.

    For details, check the CCS Build Errors page at:
    software-dl.ti.com/.../sdto_ccs_build-errors.html

    Hope this helps,
    Rafael