Part Number: CC2640R2F
Other Parts Discussed in Thread: LM335
Tool/software: Code Composer Studio
Hello
I'm doing a little project in which i use a CC2640R2 with a LM335 to measure the ambient temperature.
tempy = (((adcValue0 * 3.3 * 100 ) /4096)); Temp_final = tempy >> 10;
But my output is not right. I connect the lm335 to 5 V and my measure is ADC Raw: 2775 and Vout= 2.98V.
Did i miss anything ?
Best regards