Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
I'm working on a project and have developed a PCB with the cc2650MODA chip on it. I am trying to load my code onto it to test the board. I have read that you can use the MSP432 Launchpad as a JTAG debugger, and to test that I'm doing it correctly I'm trying to load code onto the cc2650 boosterpack first. I have the boosterpack connected to the XDS110 Out of the Launchpad, removed all jumpers to the MSP432, and shorted the Enable XDS110 Power Out, JP102 points. I am running the basic pininterrupt cc2650F128 driver from TI, the only thing that I changed was declared DIO4 as LED1 and disregarding button presses, just turn the LED on. I have gotten past all of the connection errors, but now when I run the code, it hits a termination and I was wondering if anyone could tell me why. I know that it has to be something simple that I just don't know about.