This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am using CCS Version: 6.0.1.00040. I have a free license.
When I open CCS I see "Free license" in the bottom right corner. When I launch a debug session I get the error shown below and the license information in the bottom corner of CCS changes to "Unlicensed". I am using the Spectrum Digital XDS510LC USB JTAG emulator to connect to the board containing the TMS320F2812 processor. What is the reason?
Error in CCS:
License cannot be acquired.
The Code Composure Studio license that you are using only allows the following connection types:
-XDS100 class emulators
-MSP430 connections
-simulators
-EVMs/DSKs/eZdsp kits with onboard emulation
Examples of restricted connections include:
-XDS200, XDS510 and XDS560 emulators