This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F280041: Migrating from CGT v18.1.2 to CGT v18.12.1

Part Number: TMS320F280041

Tool/software: TI C/C++ Compiler

Hello,

we have already developed some applications, using CGT v18.1.2.

Now, we are going to develop a new application based on the same microcontroller, and we were evaluating to upgrade the compiler.

We have seen that the latest version (v18.12.1) is pretty new, so we were wandering if it is a goog idea to upgrade the compiler, or if it is better to continue to use the older one.

What is your suggestion?

Is there a good reason to upgrade from 18.1.2 to 18.12.1?

Thank you,

Carlo