Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Image will not flash in CCS, and the FlashLoaderCC26x0 is located only in "C:\ti\uniflash_4.6.0\deskdb\content\TICloudAgent\win\ccs_base\arm\FlashLoaderCC26x0.out"
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Failed to write flashloader to device SRAM. Error: Unable to read algorithm file "C:\ti\ccsv8\ccs_base\DebugServer\bin\..\..\arm\FlashLoaderCC26x0.out"
Cortex_M3_0: File Loader: Memory write failed: Failed to write flashloader to device SRAM.
The image flashes w/ Uniflash and runs on the board successfully however.
Where is the setting to change the path to FlashLoaderCC26x0?
Thank you