This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: Cannot put longer serial string into XDS110 after putting a short one in using -s

Part Number: CC1310

Tool/software: Code Composer Studio

Picking on CCS 'cause there isn't a forum for the debug probes. After seeing the error of my ways by parsing the XDS110 instructions to imply no *embedded* blanks are allowed in the eight character string passed  with -s, I'm trying to change "X-NE" to "X-NE____" to conform to the spec and stop corrupting my .ccxml file in CCS-land. But here's what I'm seeing. A  workaround would be much appreciated.

~/rt1/ti/ccsv8/ccs_base/common/uscif/xds110$ xdsdfu -m 

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2018 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...


<<<< Device 0 >>>>

VID: 0x0451    PID: 0xbef3
Device Name:   XDS110 Probe with CMSIS-DAP
Version:       2.3.0.17
Manufacturer:  Texas Instruments
Serial Num:    X-NE
Mode:          Runtime
Configuration: Standard

Switching device into DFU mode.
~/rt1/ti/ccsv8/ccs_base/common/uscif/xds110$ xdsdfu -s X-NE____ 

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2018 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...

Device is in runtime mode. Switch to DFU mode using '-m' before
attempting any other operation

  • ~/rt1/ti/ccsv8/ccs_base/common/uscif/xds110$ xdsdfu -e
    
    USB Device Firmware Upgrade Utility
    Copyright (c) 2008-2018 Texas Instruments Incorporated.  All rights reserved.
    
    Scanning USB buses for supported XDS110 devices...
    
    
    <<<< Device 0 >>>>
    
    VID: 0x1cbe    PID: 0x00ff
    Device Name:   Device Firmware Update
    Manufacturer:  Texas Instruments Incorporated
    Serial Num:    1.0.0.1
    Mode:          DFU
    
    Found 1 device.
    

    Yes, the old unplug/replug trick fixed this too.