Part Number: TMS320C6713B
Tool/software: Code Composer Studio
Hello, I'm trying to use a legacy custom board with a 'c6713 (TMS320C6713B) and a Blackhawk USB200 JTAG emulator. The custom board electrically is very similar to the DSK6713.
I am successfully using CCS (v7.4.0) and a newer custom board based on a 'c6748, so I can do the basics of connecting to a new board from CCS (JTAG, ccxml, gel, etc).
When I try to set up a new ccxml Target Configuration file for the legacy C6713 board, however, I don't see the C6713 as a device option (Under "General Setup", "Board or Device"). I have also tried CCSv7, CCSv6, CCSv5, and did not see an option for C6713 devices.
But in the linked e2e post ("related question"), it sounds like there is a way to use CCS v7.4 with the C6713? How do I set up a ccxml file for C6713 and CCSv7?
Thank you very much!
Jim